:CRECovery:SSCLock
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECoveryN:SSCLock {ON | OFF | 1 | 0}
Where N identifies the slot number and must be selected from {1:8}. The slot number is associated with the N107x-series or 86108A/B Precision Waveform Analyzer module with Option JSA. When an 86108A/B module is used, the slot number is always 1.
Query Syntax
:CRECoveryN:SSCLock?
Query Response
{1 | 0}
Description
Turns on the ability to use the nominal symbol rate when recoverying the clock on Spread Spectrum Clock (SSC) signals. Normally, FlexDCA uses the average symbol rate to recovery the clock. However, when performing clock recovery on a SSC signal, using the nominal symbol rate may be required. The default setting is off.
Requires FlexDCA revision A.05.80 and above.