:SPRocess:DFEQualizer:CLKDelay
Command Syntax
:SPRocessN:DFEQualizer:CLKDelay <delay_time>
<delay_time> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:DFEQualizer:CLKDelay?
Description
Sets the time delay for a Decision Feedback Equalizer operator (DFE), which delays the decision point used by the slicer. The decision point is placed directly between the edges, so as to delay the edges.
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:CLKDelay command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:CLKDelay
The Decision Feedback Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:FUNCtion1:FOPerator DFEQualizer :FUNCtion1:DISPlay ON :FUNCtion1:COLor TCOLor9 :SPRocess1:DFEQualizer:TAPS:AUTo ON :SPRocess1:DFEQualizer:TAPS:COUNt 5 :SPRocess1:DFEQualizer:TAPS:ULIMit 4.5E-1 :SPRocess1:DFEQualizer:TAPS:LLIMit -4.5E-1 :SPRocess1:DFEQualizer:CLKDelay 4.0E-12 :SPRocess1:DFEQualizer:BANDwidth:AUTo ON :SPRocess1:DFEQualizer:DTHReshold OFF