:SPRocess:DFEQualizer:PROPtimize:BMIN

Command Syntax

:SPRocessN:DFEQualizer:PROPtimize:BMIN "limit, limit, …"

The command argument is a string of comma separated list of real numbers (limit values).

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DFEQualizer:PROPtimize:BMIN?

Description

Sets the minimum tap values (bbmin(n)) for each tap, when tap magnitude limits are off (:SPRocess:DFEQualizer:PROPtimize:LTMagnitudes OFF). To set the maximum tap values (bbmax(n)) for each tap, use the associated :SPRocess:DFEQualizer:PROPtimize:BMAX command.

For Reference Rx operator, what function do I send this command to?

If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PROPtimize:BMIN command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:DFEQualizer:PROPtimize:BMIN

Pulse response optimization (:SPRocess:DFEQualizer:PROPtimize) must be on to use this command.

Automatic taps (:SPRocess:DFEQualizer:TAPS:AUTo) can be on or off when using this command.

Requires FlexDCA revision A.06.80 and above.