:SPRocess:DFEQualizer:PROPtimize:TAPS

Command Syntax

:SPRocessN:DFEQualizer:PROPtimize:TAPS  "tap_value, tap_value, …"

The command argument is a string of comma separated list of real numbers (individual tap value).

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DFEQualizer:PROPtimize:TAPS?

Query Response

1.4582E-02,9.1E-05,1.85E-04

Description

When :SPRocess:DFEQualizer:PROPtimize is ON and :SPRocess:DFEQualizer:TAPS:AUTo is OFF, use this command to manually enter tap values for an optimized pulse response. For example, for three taps you might enter:

:DFEQualizer:PROPtimize:TAPS "1.4582E-02,9.1E-05,1.85E-04"

For Reference Rx operator, what function do I send this command to?

If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PROPtimize:TAPS command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:DFEQualizer:PROPtimize:TAPS

Pulse response optimization (:SPRocess:DFEQualizer:PROPtimize) must be on to use this command.

Requires FlexDCA revision A.06.60 and above.