:SPRocess:DFEQualizer:PRESets:SELections
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Query Syntax
:SPRocess:DFEQualizer:PRESets:SELections?
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the Decision Feedback Equalizer (DFE) operator. Use the PRESet command to load one of these presets.
DFE Operator Presets
- IEEE 802.3ck
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PRESets:SELections command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:PRESets:SELections
Requires FlexDCA revision A.04.50 and above.