:SPRocess:DFEQualizer:PRESets
Command Syntax
:SPRocess:DFEQualizer:PRESets <string>
Description
Loads a previously saved a preset for a Decision Feedback Equalizer (DFE) operator. To query which presets are available for loading, use the PRESets:SELections? query.
DFE Operator Presets
- IEEE 802.3ck
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PRESets command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:PRESets
Presets can only be saved from the operator's Setup dialog. There is no programming command for this task.
Requires FlexDCA revision A.04.50 and above.
Example Command
:SPRocess:DFEQualizer:PRESets "MyPreset" // Load a saved preset.