:SPRocess:DFEQualizer:PROPtimize:SAVE
Command Syntax
:DFEQualizer:PROPtimize:SAVE {ON | OFF}
Query Syntax
:SPRocessN:DFEQualizer:PROPtimize:SAVE?
Description
When :SPRocess:DFEQualizer:PROPtimize is ON and :SPRocess:DFEQualizer:TAPS:AUTo is ON, automatically saves the pulse-optimized waveform to a Y-values waveform text file (.txt) whenever an optimization is recalculated. The optimization is recalculated when any of the following command change a setting:
:SPRocess:DFEQualizer:TAPS:RECalculate:SPRocess:DFEQualizer:PROPtimize:DELay:SPRocess:DFEQualizer:PROPtimize:LENGth:SPRocess:DFEQualizer:PROPtimize:BMAX
Use the :SPRocess:DFEQualizer:PROPtimize:SAVE:FILE command to specify the file name used. The default file name is PulseResponse.txt.
The contents of the saved file is similar to the following listing:
File Format, WaveformYValues Format Version, 1 Instrument, N1010A SerialNumber, SwVersion, P.06.60.308 Date, 06/21/2020 09:06:01 Source Name, Channel 5A Channel Bandwidth, 15000000000 Channel Noise, 2E-06 Pulse Delay (Dp), 3 Pulse Length (Np), 200 Symbol Rate (Baud), 9953280000 Samples/UI, 30 Signal Amplitude, 0.000257699147049349 Main Cursor Index (ts), 111 Main Cursor Amplitude, 0.000250017282488446 Taps, 0.000188668491937765,9.66601087149695E-05,-7.71286501485765E-05,9.05218082888484E-05 Points, 6000 XOrg, 0 XInc, 3.34897976680384E-12 X Units, Second Y Units, Watt Data, -6.59147544236711E-07 -2.60442158837837E-07 ...
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PROPtimize:SAVE command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:PROPtimize:SAVE
Pulse response optimization (:SPRocess:DFEQualizer:PROPtimize) must be on to use this command.
Requires FlexDCA revision A.06.60 and above.
Example
The following code results in the following file:
"C:\Users\kent\Documents\Keysight\FlexDCA\Waveforms\DUT-7.txt"
:SPRocess:DFEQualizer:PROPtimize ON :SPRocess:DFEQualizer:PROPtimize:SAVE:FILE "DUT-7" :SPRocess:DFEQualizer:PROPtimize:SAVE ON