:SPRocess:DFEQualizer:PROPtimize

Command Syntax

:SPRocessN:DFEQualizer:PROPtimize {ON | OFF}

Query Syntax

:SPRocessN:DFEQualizer:PROPtimize?

Query Response

{0 | 1}

Description

Turns the DFE equalizer's pulse optimization on or off. The following table shows the:

  • child commands only have an effect when the optimization is on.
  • child commands that only have an effect when the automatic taps (:SPRocess:DFEQualizer:TAPS:AUTo) is off: :TAPS, :SAMPlitude, and :MCURsor.
  • Optimized data files can only be saved when both optimization and automatic taps (:SPRocess:DFEQualizer:TAPS:AUTo) are on.
Required Conditions for :DFEQualizer:PROPtimize: Child Commands
Child Command :DFEQ:TAPS:AUTo :DFEQ:PROPtimize Description Associated Control Tab
Location in DFE Setup Dialog
OFF ON OFF ON
:DFEQ:PROP:TAPS ■ ■ Enters the tap values. Taps
:DFEQ:PROP:SAMPlitude ■ ■ Enter the signal amplitude. Taps
:DFEQ:PROP:MCURsor ■ ■ Enters the main cursor amplitude. Taps
:DFEQ:PROP:BMAX ■ ■ ■ Enters the tap limits (bmax(N)) values. Advanced
:DFEQ:PROP:DELay ■ ■ ■ Enters the pulse delay (Dp) in UI. Pulse Response Tab
:DFEQ:PROP:LENGth ■ ■ ■ Enters the pulse length (Np) in UI. Pulse Response Tab
:DFEQ:PROP:SAVE ■ ■ Saves the pulse response to a file after optimization. Pulse Response Tab
:DFEQ:PROP:SAVE:FILE ■ ■ Specifies the file to which to save the pulse response. Pulse Response Tab

For Reference Rx operator, what function do I send this command to?

If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PROPtimize command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:DFEQualizer:PROPtimize

Requires FlexDCA revision A.06.60 and above.