:SPRocess:DFEQualizer:PROPtimize:MCURsor
Command Syntax
:SPRocessN:DFEQualizer:PROPtimize:MCURsor
Query Syntax
:SPRocessN:DFEQualizer:PROPtimize:MCURsor?
Description
When :SPRocess:DFEQualizer:PROPtimize is ON and :SPRocess:DFEQualizer:TAPS:AUTo is OFF, use this command to enter Main Cursor Amplitude for the optimized pulse response.
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:PROPtimize:MCURsor command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:PROPtimize:MCURsor
Pulse response optimization (:SPRocess:DFEQualizer:PROPtimize) must be on to use this command.
Requires FlexDCA revision A.06.60 and above.
Example
To enter 246.48 μW:
:SPRocess:DFEQualizer:PROPtimize:MCURsor "2.4648E-4"