:SPRocess:DFEQualizer:TAPS:AUTo
Command Syntax
:SPRocessN:DFEQualizer:TAPS:AUTo {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:DFEQualizer:TAPS:AUTo?
Query Response
{1 | 0}
Description
Turns on and off automatic configuration of taps for a Decision Feedback Equalizer operator (DFE). By default, automatic configuration is on.
- OFF
- Disables automatic tap configuration to enable manual entry of tap values. Use the
:SPRocess:DFEQualizer:TAPScommand to enter the individual tap values. - ON
- Enables automatic tap configuration which sets the optimum tap values to open an eye diagram. This is the default setting. To enter the number of taps, use the
:SPRocess:DFEQualizer:TAPS:COUNtcommand. Use the:SPRocess:DFEQualizer:TAPS:RECalculatecommand to automatically recalculate the tap values.
For Reference Rx operator, what function do I send this command to?
If the DFE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:DFEQualizer:TAPS:AUTo command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:DFEQualizer:TAPS:AUTo
The Decision Feedback Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.
Beginning with FlexDCA revision A.05.60, use of an *OPC? query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:FUNCtion1:FOPerator DFEQualizer :FUNCtion1:DISPlay ON :FUNCtion1:COLor TCOLor9 :SPRocess1:DFEQualizer:TAPS:AUTo ON;*OPC? :SPRocess1:DFEQualizer:TAPS:COUNt 5;*OPC? :SPRocess1:DFEQualizer:TAPS:ULIMit 4.5E-1;*OPC? :SPRocess1:DFEQualizer:TAPS:LLIMit -4.5E-1;*OPC? :SPRocess1:DFEQualizer:CLKDelay 4.0E-12 :SPRocess1:DFEQualizer:BANDwidth:AUTo OFF :SPRocess1:DFEQualizer:BANDwidth 1.0E+10 :SPRocess1:DFEQualizer:TAPS:RECalculate;*OPC? :SPRocess1:DFEQualizer:DTHReshold OFF