:SPRocess:RRX:LIMits:BALance:STATe

Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:RRX:LIMits:BALance:STATe  {ON | OFF | 1 | 0}

Query Syntax

:SPRocess:RRX:LIMits:BALance:STATe?

Query Response

{1 | 0}

Description

For the Reference Rx operator, this command turns on or off the Pre-Post Equalizer Coefficient Difference Limit. In the Reference Receiver Setup dialog, the setting is Flag if Limited or Enforce Limit, depending on the presence of a secondary DFE operator. This feature is called out in the IEEE 802.3dj 2.2/2.3 standard. The actual limit is set using the:SPRocess:RRX:LIMits:BALance:LIMit command.