:SPRocess:RRX:LIMits:FMBDfe
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RRX:LIMits:FMBDfe {ON | OFF}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function. This feature is selected in the Select Equalizers tab of the Reference Receiver Setup dialog and is identified as the Reduce FFE Main Tap min. by first DCA Tap setting.
Query Syntax
:SPRocess:RRX:LIMits:FMBDfe?
Query Response
{ON | OFF}
Description
For the Reference Rx operator, this command reduces the FFE equalizer's main tap minimum value by the value of the first DFE tap. This command is only available when the Reference Receiver operator is configured with both a TDECQ Equalizer and a DFE equalizer.