Meas Commands - Standard Measurement Class

Click here to view links to Meas commands for all Measurement Classes.

S-Param

Balanced

Receivers

Waves

Meas
Setup

S-Param Tab Commands
Softkey Sub-item SCPI COM
S11 On/Off CALCulate:MEASure:PARameter CreateS-Parameter
S21 On/Off CALCulate:MEASure:PARameter CreateS-Parameter
S12 On/Off CALCulate:MEASure:PARameter CreateS-Parameter
S22 On/Off CALCulate:MEASure:PARameter CreateS-Parameter
Other... S11, S12, S13, S14, S21, S22, S23, S24, S31, S32, S33, S34, S41, S42, S43, S44 CALCulate:MEASure:PARameter CreateS-Parameter
S-Parameter CALCulate:MEASure:PARameter CreateS-Parameter
Balanced CALCulate:MEASure:PARameter BalSMeasurement BBalMeasurement BSSMeasurement SBalMeasurement SSBMeasurement
Receivers CALCulate:MEASure:PARameter CreateS-Parameter
Meas Class...   CALCulate:MEASure:DEFine CreateCustomMeasurementEx
Meas Class... (TDR only)   SYSTem:TDR:INITialize None
Balanced Tab Commands
Softkey Sub-item SCPI COM
Sss11 On/Off CALCulate:MEASure:PARameter BalSMeasurement
Sds21 On/Off CALCulate:MEASure:PARameter BalSMeasurement
Ssd12 On/Off CALCulate:MEASure:PARameter BalSMeasurement
Sdd22 On/Off CALCulate:MEASure:PARameter BalSMeasurement
Other... Sdd11, Scd11, Sdc11, Scc11, Ssd21, Ssc21, Sds12, Scs12, Sss22 CALCulate:MEASure:PARameter BalSMeasurement
Sdd11, Sdd12, Sdd22, Scd11, Scd12, Scd21, Scd22, Sdc11, Sdc12, Sdc21, Sdc22, Scc11, Scc12, Scc21, Scc22 CALCulate:MEASure:PARameter BBalMeasurement
Sdd11, Scd11, Sdc11, Scc11,
Ssd21, Ssc21, Ssd31, Ssc31,
Sds12, Sds13, Scs12, Scs13,
Sss22, Sss32, Sss23, Sss33
CALCulate:MEASure:PARameter BSSMeasurement
Sss11, Ssd12, Ssc12, Sds21, Scs21, Sdd22, Sdc22, Scd22, Scc22 CALCulate:MEASure:PARameter SBalMeasurement
Sss11, Sss12, Sss21, Sss22, Ssd13, Ssc13, Ssd23, Ssc23, Sds31, Sds32, Scs31, Scs32, Sdd33, Sdc33, Scd33, Scc33 CALCulate:MEASure:PARameter SSBMeasurement
S-Parameter CALCulate:MEASure:PARameter CreateS-Parameter
Balanced CALCulate:MEASure:PARameter BBalMeasurement
Receivers CALCulate:MEASure:PARameter App.CreateCustomMeasurementEx
Topology... Topology Tab
BAL CALCulate:FSIMulator:BALun:DEVice SetBPort
BAL-BAL CALCulate:FSIMulator:BALun:DEVice SetBBPorts
BAL-SE CALCulate:FSIMulator:BALun:DEVice SetBSPorts
BAL-SE-SE CALCulate:FSIMulator:BALun:DEVice SetBSSPorts
SE-BAL CALCulate:FSIMulator:BALun:DEVice SetSBPorts
SE-SE-BAL CALCulate:FSIMulator:BALun:DEVice SetSSBPorts
Custom CALCulate:FSIMulator:BALun:DEVice SetCustomDUTTopology
Balanced Port

(set specific port)

(for systems with >4 ports)

  CALCulate:FSIMulator:BALun:BPORt:STIMulus:TRUe:STATe CALCulate:DTOPology   BalancedPortTrueState

SetCustomDUTTopology

Balanced Port (logical port) VNA (+)Port (physical port) VNA (-)Port (physical port) CALCulate:FSIMulator:BALun:TOPology:BALanced[:PPORts] CALCulate:FSIMulator:BALun:TOPology:BALSended[:PPORts] CALCulate:FSIMulator:BALun:TOPology:BBALanced[:PPORts] CALCulate:FSIMulator:BALun:TOPology:BSSended[:PPORts] CALCulate:FSIMulator:BALun:TOPology:SBALanced[:PPORts] CALCulate:FSIMulator:BALun:TOPology:SSBalanced[:PPORts] SetBPort SetBSPorts SetBBPorts SetBSSPorts SetSBPorts SetSSBPorts
True Mode CALCulate:FSIMulator:BALun:STIMulus:MODE Mode
Port Z Tab
Enable Differential Z Conversion CALCulate:FSIMulator:BALun:DZConversion:STATe

DiffZConvState

Enable Common Z Conversion CALCulate:FSIMulator:BALun:CZConversion:STATe

CmnModeZConvState

Enable SE Port Z Conversion CALCulate:FSIMulator:SENDed:ZCONversion:STATe

PortArbzState

Complex Z Wave Normalization SENSe<cnum>:CORRection:WAVE:NORM[:METHod]

None

Converted Z Real CALCulate:FSIMulator:BALun:CZConversion:BPORt:REAL

PortArbzReal

Converted Z Imaginary CALCulate:FSIMulator:BALun:CZConversion:BPORt:IMAG

PortArbzImag

Offset Tab

Apply Power Offset As Fixture

CALCulate:FSIMulator:BALun:FIXTure:OFFSet:POWer

PowerAsFixture

Apply Phase Offset As Fixture

CALCulate:FSIMulator:BALun:FIXTure:OFFSet:PHASe

PhaseAsFixture

Power Offset

CALCulate:FSIMulator:BALun:BPORt:OFFSet:POWer

 

CALCulate:FSIMulator:BALun:LPORt:OFFSet:POWer

BalPort1PowerOffset

BalPort2PowerOffset

None

Phase Offset

CALCulate:FSIMulator:BALun:BPORt:OFFSet:PHASe

 

CALCulate:FSIMulator:BALun:LPORt:OFFSet:PHASe

BalPort1PhaseOffset

BalPort2PhaseOffset

None

Sweep Tab

Select Active Source

CALCulate:FSIMulator:BALun:PHASe:SWEep:PORT

None

Enable Balanced Phase Sweep

CALCulate:FSIMulator:BALun:PHASe:SWEep:STATe

PhaseSwpState

  Start Phase

CALCulate:FSIMulator:BALun:BPORt:SWEep:PHAse:STARt

 

CALCulate:FSIMulator:BALun:LPORt:SWEep:PHAse:STARt

BalPort1StartPhase

BalPort2StartPhase

None

  Stop Phase

CALCulate:FSIMulator:BALun:BPORt:SWEep:PHAse:STOP

 

CALCulate:FSIMulator:BALun:LPORt:SWEep:PHAse:STOP

BalPort1StopPhase

BalPort2StopPhase

None

  Offset as fixture

CALCulate:FSIMulator:BALun:FIXTure:PHASe

PhaseSwpAsFixture

Enable Differential Source Only Mode

CALCulate:FSIMulator:BALun:STIMulus:MODE

Mode

Receivers Tab Commands
Softkey Sub-item SCPI COM
A Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
A Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
B Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
B Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
R1 Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
R2 Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
Other... (A,1), (A,2), (A,3), (A,4), (B,1), (B,2), (B,3), (B,4), (C,1), (C,2), (C,3), (C,4), (D,1), (D,2), (D,3), (D,4), (R1,1), (R2,2), (R3,3), (R4,4) CALCulate:MEASure:PARameter CreateCustomMeasurementEx
S-Parameter CALCulate:MEASure:PARameter CreateS-Parameter
Balanced CALCulate:MEASure:PARameter BBalMeasurement
Receivers CALCulate:MEASure:PARameter CreateCustomMeasurementEx
Waves Tab Commands
Softkey Sub-item SCPI COM
a1 Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
a2 Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
b1 Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
b1 Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
b2 Source Port 1 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
b2 Source Port 2 On/Off CALCulate:MEASure:PARameter CreateCustomMeasurementEx
Other... (a1,1), (a2,2), (a3,3), (a4,4), (b1,1), (b1,2), (b1,3), (b1,4), (b2,1), (b2,2), (b2,3), (b2,4), (b3,1), (b3,2), (b3,3), (b3,4), (b4,1), (b4,2), (b4,3), (b4,4) CALCulate:MEASure:PARameter CreateCustomMeasurementEx
S-Parameter CALCulate:MEASure:PARameter CreateS-Parameter
Balanced CALCulate:MEASure:PARameter BBalMeasurement
Receivers CALCulate:MEASure:PARameter CreateCustomMeasurementEx
COM
CreateCustomMeasurementEx
CreateCustomMeasurementEx
CreateCustomMeasurementEx
CreateCustomMeasurementEx
CreateCustomMeasurementEx
CreateS-Parameter
BBalMeasurement
CreateCustomMeasurementEx
Meas Setup Tab Commands
Softkey Sub-item SCPI COM
Conversions Off CALCulate:MEASure:CONVersion:FUNCtion None
Z-Reflect CALCulate:MEASure:CONVersion:FUNCtion None
Z-Transmit CALCulate:MEASure:CONVersion:FUNCtion None
Z-Trans-Shunt CALCulate:MEASure:CONVersion:FUNCtion None
Y-Reflect CALCulate:MEASure:CONVersion:FUNCtion None
Y-Transmit CALCulate:MEASure:CONVersion:FUNCtion None
Y-Trans-Shunt CALCulate:MEASure:CONVersion:FUNCtion None
1 / S CALCulate:MEASure:CONVersion:FUNCtion None
Conjugation CALCulate:MEASure:CONVersion:FUNCtion None
Correction Channel Correction On SENSe:CORRection[:STATe] ErrorCorrection
Channel Correction Off

SENSe:CORRection[:STATe]

ErrorCorrection

Cal Set...

 

 

Basic Cal...

 

 

Smart Cal...

 

 

Trace Hold Off CALCulate:MEASure:HOLD:TYPE TraceHoldType
Max CALCulate:MEASure:HOLD:TYPE TraceHoldType
Min CALCulate:MEASure:HOLD:TYPE TraceHoldType
Restart CALCulate:MEASure:HOLD:CLEar TraceHoldClear
Equation Editor... On/Off CALCulate:MEASure:EQUation[:STATe] State
Equation CALCulate:MEASure:EQUation:TEXT Text
Enable Equation CALCulate:MEASure:EQUation[:STATe] State
Functions CALCulate:EQUation:LIBRary:FUNCtions GetLibraryFunctions
Trace Data None None
Parameter None None
Store Equation None None
Delete Equation None None
Use Short Names None None
Enable Matlab None None
Import... None None
    Import Library CALCulate:EQUation:LIBRary:IMPort ImportLibrary
    Remove Library CALCulate:EQUation:LIBRary:REMove RemoveLibrary
Memory... Data->Memory CALCulate:MEASure:MATH:MEMorize DataToMemory
Data Math
Off CALCulate:MEASure:MATH:FUNCtion TraceMath
Data / Memory CALCulate:MEASure:MATH:FUNCtion TraceMath
Data * Memory CALCulate:MEASure:MATH:FUNCtion TraceMath
Data - Memory CALCulate:MEASure:MATH:FUNCtion TraceMath
Data + Memory CALCulate:MEASure:MATH:FUNCtion TraceMath
8510 Mode None None
Trace View Options
Data Trace DISPlay:WINDow:TRACe[:STATe] View
Memory Trace DISPlay:WINDow:TRACe:MEMory View
Data and Memory Trace DISPlay:WINDow:TRACe[:STATe] DISPlay:WINDow:TRACe:MEMory View
Time Domain... Transform
Transform On CALCulate:MEASure:TRANsform:TIME:STATe State
Start CALCulate:MEASure:TRANsform:TIME:STARt Start
Stop CALCulate:MEASure:TRANsform:TIME:STOP Stop
Center CALCulate:MEASure:TRANsform:TIME:CENTer Center
Span CALCulate:MEASure:TRANsform:TIME:SPAN Span
Low Pass Impulse CALCulate:MEASure:TRANsform:TIME[:TYPE] Mode
Low Pass Step CALCulate:MEASure:TRANsform:TIME[:TYPE] Mode
Band Pass CALCulate:MEASure:TRANsform:TIME[:TYPE] Mode
Set Low Pass Frequencies CALCulate:MEASure:TRANsform:TIME:LPFREQuency SetFrequencyLowPass
Gating
Gating On CALCulate:MEASure:FILTer[:GATE]:TIME:STATe State
Start CALCulate:MEASure:FILTer[:GATE]:TIME:STARt Start
Stop CALCulate:MEASure:FILTer[:GATE]:TIME:STOP Stop
Center CALCulate:MEASure:FILTer[:GATE]:TIME:CENTer Center
Span CALCulate:MEASure:FILTer[:GATE]:TIME:SPAN Span
Gate Type CALCulate:MEASure:FILTer[:GATE]:TIME[:TYPE] Type
Gate Shape CALCulate:MEASure:FILTer[:GATE]:TIME:SHAPe Shape
Window
Minimum/Maximum DISPlay:WINDow:SIZE app.WindowState
Kaiser Beta CALCulate:MEASure:TRANsform:TIME:KBESsel KaiserBeta
Impulse Width CALCulate:MEASure:TRANsform:TIME:IMPulse:WIDTh ImpulseWidth
Coupling
Coupling On SENSe:COUPle:PARameter[:STATe] CoupleChannelParams
Transform Parameters
    Stimulus CALCulate:MEASure:TRANsform:COUPle:PARameters CoupledParameters
    State (On/Off) CALCulate:MEASure:TRANsform:COUPle:PARameters CoupledParameters
    Window CALCulate:MEASure:TRANsform:COUPle:PARameters CoupledParameters
    Mode CALCulate:MEASure:TRANsform:COUPle:PARameters CoupledParameters
    Distance Marker Unit CALCulate:MEASure:TRANsform:COUPle:PARameters CoupledParameters
Gating Parameters
    Stimulus CALCulate:MEASure:FILTer[:GATE]:COUPle:PARameters CoupledParameters (Gating)
    State (On/Off) CALCulate:MEASure:FILTer[:GATE]:COUPle:PARameters CoupledParameters (Gating)
    Shape CALCulate:MEASure:FILTer[:GATE]:COUPle:PARameters CoupledParameters (Gating)
    Type CALCulate:MEASure:FILTer[:GATE]:COUPle:PARameters CoupledParameters (Gating)
Marker
Auto CALCulate:MEASure:TRANsform:TIME:MARKer:MODE DistanceMarkerMode
Reflection (divide by 2) CALCulate:MEASure:TRANsform:TIME:MARKer:MODE DistanceMarkerMode
Transmission CALCulate:MEASure:TRANsform:TIME:MARKer:MODE DistanceMarkerMode
Meters (m) CALCulate:MEASure:TRANsform:TIME:MARKer:UNIT DistanceMarkerUnit
Feet (ft) CALCulate:MEASure:TRANsform:TIME:MARKer:UNIT DistanceMarkerUnit
Inches (in) CALCulate:MEASure:TRANsform:TIME:MARKer:UNIT DistanceMarkerUnit
Velocity Factor

SENSe:CORRection:EXTension:PORT:VELFactor

VelocityFactor