:FUNCtion:TBASe:RFALl:METHod

Command Syntax

:FUNCtionN:TBASe:RFALl:METHod  {AUTO | ABSolute}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:TBASe:RFALl:METHod?

Description

For the indicated function, selects the method used to define the waveform top and base definitions. The command is equivalent to setting the signal's Top-Base Definition in the Thresholds > Rise/Fall tab of the Configure Measurements dialog box.

AUTO
Specifies that the top (100%) and base (0%) levels be automatically determined using a histogram of the signal's amplitude values. This is the default setting.
ABSolute
Allows you to enter absolute values for the top-base levels. When ABSolute is selected, use the :FUNCtion:THReshold:RFALl:TOP and :FUNCtion:THReshold:RFALl:BASE commands to enter the signal's top and base levels.

Example Command Sequence

:FUNCtion3:THReshold:RFALl:TRACking OFF
:FUNCtion3:TBASe:RFALl:METHod ABSolute
:FUNCtion3:THReshold:RFALl:BASE -125E-3
:FUNCtion3:THReshold:RFALl:TOP 125E-3