:FUNCtion:THReshold:GENeral:PAM:ASTHresholds
Command Syntax
:FUNCtionN:THReshold:GENeral:PAM:ASTHresholds
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Description
When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :FUNCtion:THReshold:GENeral:METHod), you can send this command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.
The automatically determined PAM thresholds and hysteresis values can be adjusted using the :FUNCtion:THReshold:GENeral:PAM:THResholds:EYE and :FUNCtion:THReshold:GENeral:HYSTeresis commands.