:FUNCtion:THReshold:RFALl:BASE

Command Syntax

:FUNCtionN:THReshold:RFALl:BASE<amplitude>

<amplitude> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:RFALl:BASE?

Description

For the indicated function, sets or queries the Rise/Fall threshold's custom base-level setting. The top and base levels are used to locate a waveform's lower and upper threshold levels for the rise time, fall time, and slew rate measurements. Specify the level in volts or Watts depending on the waveform type. Use :FUNCtion:THReshold:RFALl:TOP to set or query a custom top level.

Before this user-defined base level can be applied to measurements, use the :FUNCtion:TBASe:RFALl:METHod command to select user-defined top-base definitions.

Example Command Sequence

:FUNCtion3:THReshold:RFALl:TRACking OFF
:FUNCtion3:TBASe:RFALl:METHod ABSolute
:FUNCtion3:THReshold:RFALl:BASE -125E-3
:FUNCtion3:THReshold:RFALl:TOP 125E-3