:FUNCtion:THReshold:RFALl:LOWer
Command Syntax
:FUNCtionN:THReshold:RFALl:LOWer <amplitude>
<amplitude> is a double.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion1{N}:THReshold:RFALl:LOWer?
Description
Sets or queries the Rise/Fall threshold's lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :FUNCtion:THReshold:RFALl:PLOWer command.
Use the :FUNCtion:THReshold:RFALl:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :FUNCtion:THReshold:RFALl:UPPer command to enter a upper threshold level.
Example Command Sequence
:FUNCtion2:THReshold:RFALl:TRACking OFF :FUNCtion2:THReshold:RFALl:METHod ABSolute :FUNCtion2:THReshold:RFALl:UPPer 125E-3 :FUNCtion2:THReshold:RFALl:LOWer -125E-3