:FUNCtion:THReshold:GENeral:BASE
Command Syntax
:FUNCtionN:THReshold:GENeral:BASE<amplitude>
<amplitude> is a double.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:THReshold:GENeral:BASE?
Description
For the indicated function, sets or queries the General threshold's custom base-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts or Watts depending on the waveform type. Use :FUNCtion:THReshold:GENeral:TOP to set or query a custom top level.
Before this user-defined base level can be applied to measurements, use the :FUNCtion:TBASe:GENeral:METHod command to select user-defined top-base definitions.
Example Command Sequence
:FUNCtion3:THReshold:GENeral:TRACking OFF :FUNCtion3:TBASe:GENeral:METHod ABSolute :FUNCtion3:THReshold:GENeral:BASE -125E-3 :FUNCtion3:THReshold:GENeral:TOP 125E-3