:FUNCtion:THReshold:GENeral:METHod

Command Syntax

:FUNCtionN:THReshold:GENeral:METHod  {P105090 | P205080 | P405060 | PERCent | HYSTeresis | ABSolute}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:METHod?

Description

Selects the upper, middle, and lower waveform threshold definitions using the following arguments:

P105090
Specifies threshold levels as 10%, 50%, and 90% values between top and base.
P205080
Specifies threshold levels as 20%, 50%, and 80% values between top and base.
P405060
Specifies threshold levels as 40%, 50%, and 60% values between top and base.
PERCent
Specifies thresholds as custom percentages between top and base. To specify the percent values for the upper, middle, and lower thresholds, use the :FUNCtion:THReshold:GENeral:PUPPer, :FUNCtion:THReshold:GENeral:PMIDdle, and :FUNCtion:THReshold:GENeral:PLOWer commands.
HYSTeresis
Specifies thresholds as a middle level value and a ±hysteresis value. The upper limit for the measurement is the middle level plus the hysteresis value. The lower limit for the measurement is the middle level minus the hysteresis value. To specify the middle and ±hysteresis values, use the :FUNCtion:THReshold:GENeral:MIDDle and :FUNCtion:THReshold:GENeral:HYSTeresis commands.
ABSolute
Specifies thresholds as absolute upper, middle, and lower vertical values. To specify the values, use the :FUNCtion:THReshold:GENeral:UPPer, :FUNCtion:THReshold:GENeral:MIDDle, and :FUNCtion:THReshold:GENeral:LOWer commands.
Selects custom user-defined threshold definitions based on absolute unit amplitudes.

Example Command Sequence

:FUNCtion2:THReshold:GENeral:TRACking OFF
:FUNCtion2:THReshold:GENeral:METHod ABSolute
:FUNCtion2:THReshold:GENeral:UPPer 125E-3
:FUNCtion2:THReshold:GENeral:MIDDle 0E0
:FUNCtion2:THReshold:GENeral:LOWer -125E-3