:FUNCtion:THReshold:GENeral:STZero

Command Syntax

:FUNCtionN:THReshold:GENeral:STZero  {{ON | 1} | {OFF | 0}}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:STZero?

Query Response

{1 | 0}

Description

When you select the ± Hysteresis threshold definition for the selected signal (see :FUNCtion:THReshold:GENeral:METHod), you can turn ON the :FUNCtion:THReshold:GENeral:STZero setting to move thresholds within ±10 mV to zero. This feature is useful for differential signals.