:FUNCtion:THReshold:RFALl:METHod
Command Syntax
:FUNCtionN:THReshold:RFALl:METHod {P1090 | P2080 | PERCent | ABSolute}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:THReshold:RFALl:METHod?
Description
Selects the upper and lower waveform threshold definitions using the following arguments:
- P1090
- Specifies threshold levels as 10% and 90% values between top and base.
- P2080
- Specifies threshold levels as 20% and 80% values between top and base.
- PERCent
- Specifies thresholds as custom percentages between top and base. To specify the percent values for the upper, middle, and lower thresholds, use the
:FUNCtion:THReshold:RFALl:PUPPerand:FUNCtion:THReshold:RFALl:PLOWercommands. - ABSolute
- Specifies thresholds as absolute upper, middle, and lower vertical values. To specify the values, use the
:FUNCtion:THReshold:RFALl:UPPerand:FUNCtion:THReshold:RFALl:LOWercommands. - Selects custom user-defined threshold definitions based on absolute unit amplitudes.
Example Command Sequence
:FUNCtion2:THReshold:RFALl:TRACking OFF :FUNCtion2:THReshold:RFALl:METHod ABSolute :FUNCtion2:THReshold:RFALl:UPPer 125E-3 :FUNCtion2:THReshold:RFALl:LOWer -125E-3