:FUNCtion:THReshold:RFALl:PAM:PAMLevels:LEVel

Command Syntax

:FUNCtionN:THReshold:RFALl:PAM:PAMLevels:LEVel{0:3}  <amplitude>

Where <amplitude> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:RFALl:PAM:PAMLevels:LEVel{0:3}?

Description

When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :FUNCtion:TBASe:RFALl:METHod), this command sets or queries the PAM level values.

Use the :FUNCtion:THReshold:RFALl:PAM:ASLevels command to automatically set the PAM levels.