:FUNCtion:THReshold:GENeral:HYSTeresis

Command Syntax

:FUNCtionN:THReshold:GENeral:HYSTeresis   <plus_or_minus_value>

<plus_or_minus_value> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:HYSTeresis?

Description

When the :FUNCtion:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source.

Use the :FUNCtion:THReshold:GENeral:MIDDle command to enter the center threshold level.

Example Command Sequence

:FUNCtion3:THReshold:GENeral:TRACking OFF
:FUNCtion3:THReshold:GENeral:METHod HYSTeresis
:FUNCtion3:THReshold:GENeral:HYSTeresis 125E-3
:FUNCtion3:THReshold:GENeral:MIDDle 0E0