:FUNCtion:THReshold:GENeral:TRACking
Command Syntax
:FUNCtionN:THReshold:GENeral:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:THReshold:GENeral:TRACking?
Query Response
{1 | 0}
Description
Specifies whether a signal tracks the General threshold's global threshold definition or uses its own threshold definition.
The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).
Example Command Sequence
:FUNCtion2:THReshold:GENeral:TRACking OFF :FUNCtion2:THReshold:GENeral:METHod ABSolute :FUNCtion2:THReshold:GENeral:UPPer 125E-3 :FUNCtion2:THReshold:GENeral:MIDDle 0E0 :FUNCtion2:THReshold:GENeral:LOWer -125E-3