:FUNCtion:THReshold:RFALl:PUPPer

Command Syntax

:FUNCtionN:THReshold:RFALl:PUPPer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:RFALl:PUPPer?

Description

When the threshold method is a custom PERCent between top and base (see :FUNCtion:THReshold:RFALl:METHod), the :FUNCtion:THReshold:RFALl:PUPPer command sets or queries the custom upper percent value.

Example Command Sequence

:FUNCtion2:THReshold:RFALl:TRACking OFF
:FUNCtion2:THReshold:RFALl:METHod PERCent
:FUNCtion2:THReshold:RFALl:PUPPer 125E-3
:FUNCtion2:THReshold:RFALl:PLOWer -125E-3