:FUNCtion:THReshold:GENeral:UPPer

Command Syntax

:FUNCtionN:THReshold:GENeral:UPPer   <amplitude>

<amplitude> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:UPPer?

Description

Sets or queries the General threshold's upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :FUNCtion:THReshold:GENeral:PUPPer command.

Use the :FUNCtion:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.

Use the :FUNCtion:THReshold:GENeral:MIDDle command to enter a middle threshold level. Use the :FUNCtion:THReshold:GENeral:LOWer command to enter a lower threshold level.

Example Command Sequence

:FUNCtion3:THReshold:GENeral:TRACking OFF
:FUNCtion3:THReshold:GENeral:METHod ABSolute
:FUNCtion3:THReshold:GENeral:UPPer 125E-3
:FUNCtion3:THReshold:GENeral:MIDDle 0E0
:FUNCtion3:THReshold:GENeral:LOWer -125E-3