:FUNCtion:THReshold:GENeral:PAM:THResholds:EYE

Command Syntax

:FUNCtionN:THReshold:GENeral:PAM:THResholds:EYE{0:2}  <amplitude>

Where <amplitude> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:PAM:THResholds:EYE{0:2}?

Description

When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :FUNCtion:THReshold:GENeral:METHod), this command sets or queries the PAM eye threshold level. This value is used when making measurements.

Use the :FUNCtion:THReshold:GENeral:HYSTeresis command to specify the amount of hysteresis.

Use the :FUNCtion:THReshold:GENeral:PAM:ASTHresholds command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.