:FUNCtion:THReshold:GENeral:TOP

Command Syntax

:FUNCtionN:THReshold:GENeral:TOP   <amplitude>

<amplitude> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:THReshold:GENeral:TOP?

Description

For the indicated function, sets or queries the General threshold's custom top-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts or Watts depending on the waveform type. Use :FUNCtion:THReshold:GENeral:BASE to set or query a custom base level.

Before this user-defined top level can be applied to measurements, use the :FUNCtion:TBASe:GENeral:METHod command to select user-defined top-base definitions.

Example Command Sequence

:FUNCtion3:THReshold:GENeral:TRACking OFF
:FUNCtion3:TBASe:GENeral:METHod ABSolute
:FUNCtion3:THReshold:GENeral:BASE -125E-3
:FUNCtion3:THReshold:GENeral:TOP 125E-3