:FUNCtion:THReshold:GENeral:AUTO
Command Syntax
:FUNCtionN:THReshold:GENeral:AUTO
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :FUNCtion:THReshold:GENeral:METHod), you can send :FUNCtion:THReshold:GENeral:AUTO to automatically set the Center Threshold (:FUNCtion:THReshold:GENeral:MIDDle) to be halfway between Vmin and Vmax and the Hysteresis value (:FUNCtion:THReshold:GENeral:HYSTeresis) to be ±0.05(Vmax - Vmin).