:FUNCtion:THReshold:RFALl:PAM:ASLevels

Command Syntax

:FUNCtionN:THReshold:RFALl:PAM:ASLevels

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Description

When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :FUNCtion:TBASe:RFALl:METHod), you can send this command to automatically set the PAM levels.

The automatically determined PAM levels can be adjusted using the :FUNCtion:THReshold:RFALl:PAM:PAMLevels:LEVel command.