:FUNCtion:THReshold:RFALl:PLOWer
Command Syntax
:FUNCtionN:THReshold:RFALl:PLOWer <percent>
<percent> is a decimal number from -25.0 to +125.0.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:THReshold:RFALl:PLOWer?
Description
When the threshold method is a custom PERCent between top and base (see :FUNCtion:THReshold:RFALl:METHod), the :FUNCtion:THReshold:RFALl:PLOWer command sets or queries the custom lower percent value.
Example Command Sequence
:FUNCtion2:THReshold:RFALl:TRACking OFF :FUNCtion2:THReshold:RFALl:METHod PERCent :FUNCtion2:THReshold:RFALl:PUPPer 125E-3 :FUNCtion2:THReshold:RFALl:PLOWer -125E-3