:FUNCtion:THReshold:GENeral:MIDDle
Command Syntax
:FUNCtionN:THReshold:GENeral:MIDDle <amplitude>
<amplitude> is a double.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:THReshold:GENeral:MIDDle?
Description
Sets or queries the middle threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :FUNCtion:THReshold:GENeral:PMIDdle command.
Use the :FUNCtion:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :FUNCtion:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :FUNCtion:THReshold:GENeral:LOWer command to enter a lower threshold level.
Example Command Sequence
:FUNCtion5:THReshold:GENeral:TRACking OFF :FUNCtion5:THReshold:GENeral:METHod ABSolute :FUNCtion5:THReshold:GENeral:UPPer 125E-3 :FUNCtion5:THReshold:GENeral:MIDDle 0E0 :FUNCtion5:THReshold:GENeral:LOWer -125E-3