:CRECovery:OUTPut:DMODe
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECovery{1:8}:OUTPut:DMODe {NORMal | SWAPped}
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module.
Query Syntax
:CRECovery{1:8}:OUTPut:DMODe?
Description
On the N4877A Clock Data Recovery and Demultiplexer extended module, this command swaps the data that is routed to the front-panel DEMUX DATA output ports. This is the output of the demultiplexer. For example, consider if the N4877A input signal is a repeating 10101010
pattern and the output at port OUT1 is 11111…
and the output port at OUT2 is 00000…
. Using this command with the SWAPped
argument would swap the outputs so that the output at OUT1 is 00000…
and the output at OUT2 is 11111…
.

Requires FlexDCA revision A.02.00 and above.