:DISPlay:ANIMation
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:ANIMation {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:ANIMation?
Query Response
{1 | 0}
Description
Turns on and off graphics animation which is visible whenever you switch FlexDCA's operating modes. A high level of graphics capability must be present. The N1000A always has high graphics capability. When FlexDCA is running on a PC, use the :DISPlay:GPERformance command to test for the level of graphics capability.
While mode switching animation affects the transition of user interface elements, it does not affect measurement capability or features. Use the :DISPlay:MANimation command to select from among the following animations:
- Rotate Toolbar
- Fade Toolbar
- Slide Toolbar
- Rotate UI
- Fade UI
- Slide UI Down
- Slide UI Right
- Scale UI
- Scale and Rotate UI
You can also check the PC's graphics performance level (must be HIGH) as shown in the About N1010A dialog.
Example Command Sequence
:DISPlay:GPERformance? … … :DISPlay:ANIMation? :DISPlay:MANimation RTOolbar