:DISPlay:CGSPectrum
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:CGSPectrum {STANdard | LCCLassic | HCCLassic | THERmal}
Query Syntax
:DISPlay:CGSPectrum?
Query Response
{STAN | LCCL | HCCL | THER}
Description
Selects the colors used to present Color Grade persistence waveforms. To select the color-grade persistence mode, use the :DISPlay:PERSistence command. The following pictures show the available color schemes that you can select. The default color scheme is Classic High Colors (HCCLassic).
Classic High Colors (HCCLassic)
Classic Low Colors (LCCLassic)
Standard Colors (STANdard)
Thermal Colors (THERmal)
To change the colors for gray scale persistence, use the :DISPlay:GSSPectrum command.
Requires FlexDCA revision A.01.80 and above.
Example Command Sequence
:DISPlay:CGSPectrum STANdard