:DISPlay:VKSignal
Instrument:
86100D
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:VKSignal {CHANnel{N} | DIFF{1:4} | FUNCtion{1:16} | WMEMory{1:8}}
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:DISPlay:VKSignal?
Description
When running FlexDCA embedded on an 86100D, selects a displayed channel, differential signal, function, or waveform memory as the focus of the front-panel vertical scale knob.