:DISPlay:TMASk
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:TMASk MASK{1:16}
Query Syntax
:DISPlay:TMASk?
Description
Up to 16 eye mask tests can be running at the same time. When multiple eye mask test are displayed, use this command to select which eye mask test results are display in the Mask Test results table. Masks are numbered in the order that they are created. Use the :DISPlay:WINDow:MTESt:LOCation command to specify the location of the panel.
To run an eye mask test, use the :MTESt{1:16}LOAD command.
Requires FlexDCA revision A.03.00 and above.