:DISPlay:CONNect:AUTo
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:CONNect:AUTo {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:CONNect:AUTo?
Query Response
{1 | 0}
Description
Turns on or off the automatic connection of data points based on the type of displayed waveform. When automatic connection is turned off, use the DISPlay:CONNect to manually connect the data points.