:DISPlay:MANimation
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:MANimation {RTOolbar | FTOolbar | STOolbar | RUI | FUI | SUDown | SURight | SUI | SARui | NANimation}
Query Syntax
:DISPlay:MANimation?
Description
Select the type of mode switching animation that is visible whenever FlexDCA is switched between Oscilloscope, Eye/Mask, or Jitter/Noise modes. Animation must be turned on with the :DISPlay:ANIMation command before the selected type of animation will be applied. Select from the following animations:
| Animation | Command Argument |
|---|---|
| Rotate Toolbar | RTOolbar |
| Fade Toolbar | FTOolbar |
| Slide Toolbar | STOolbar |
| Rotate UI | RUI |
| Fade UI | FUI |
| Slide UI Down | SUDown |
| Slide UI Right | SURight |
| Scale UI | SUI |
| Scale and Rotate UI | SARui |
| No Animation UI | NANimation |
Example Command Sequence
:DISPlay:GPERformance? … … :DISPlay:ANIMation? :DISPlay:MANimation RTOolbar