:DISPlay:GPERformance?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexOTO
Query Syntax
:DISPlay:GPERformance?
Description
Queries the level of graphics support in your PC: LOW, MED, or HIGH. The level on a DCA-X's is always HIGH.
The level for FlexDCA on a DCA-X's is always HIGH. FlexDCA's mode-switching animation requires that the graphics support level be HIGH. To turn on and off mode-switching animation use the :DISPlay:ANIMation command. Animation is visible whenever you switch FlexDCA's operating modes. For example, when you switch from Eye/Mask mode to Jitter/Noise mode. Mode-switching animation affects the transition of user interface elements, but does not affect measurement capability or features. Select from among the following animations using the :DISPlay:MANimation command:
- Rotate Toolbar
- Fade Toolbar
- Slide Toolbar
- Rotate UI
- Fade UI
- Slide UI Down
- Slide UI Right
- Scale UI
- Scale and Rotate UI
Example Command Sequence
:DISPlay:GPERformance? … … :DISPlay:ANIMation? :DISPlay:MANimation RTOolbar