:DISPlay:CTHeme
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISPlay:CTHeme {"Tungsten" | "Aluminum"}
Query Syntax
:DISPlay:CTHeme?
Description
Selects one of two user-interface themes that affects the look of FlexDCA's window and dialogs. The placing of double or single quotes around the string argument is required. Tungsten is the Factory Preset theme. A Default Setup does not change the selected theme.
This command supports the DEFault common child command.