:DISPlay:CONNect
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:CONNect {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:CONNect?
Query Response
{1 | 0}
Description
Turns on or off the display of lines connecting consecutive data points on the display. This allows you to view what the waveform actually looks like. This command is available in Oscilloscope mode with persistence (:DISPlay:PERSistence) set to minimum, infinite, or variable. It is not available in Eye/Mask mode. By default, the decision to connect the data points is automatically made (DISPlay:CONNect:AUTo) based on the type of displayed waveform. You can always clear this setting to manually turn this feature on or off.