:DISPlay:SPPanel
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:SPPanel {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:SPPanel?
Query Response
{1 | 0}
Description
Hides (OFF) or displays (ON) the signal-processing Math palette. This is identical to clicking the Math button that is located in the applications bottom-right corner. The default setting is OFF. To hide or show the Signals palette, use the DISPlay:SPALette command.