:MEASure:TDEQ:PRESets:SELections?
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:TDEQ:PRESets:SELections?
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the TDECQ measurement (:MEASure:EYE:TDEQ). Use the :MEASure:TDEQ:PRESet command to load a preset.
Ref. Rx Equalizer Presets
- IEEE 802.3dj Draft 2.3
- CEI-112G-Linear TP1a (53GBd)
- CEI-112G-Linear TP4 (53GBd)
- IEEE 802.3dj Draft 2.0
- IEEE 802.3bs Amended
- IEEE 802.3bs
- IEEE 802.3cd
- IEEE 802.3db SR SECQ
- IEEE 802.3db SR (844-863 nm)
- IEEE 802.3db VR (842-948 nm)
- IEEE 802.3db VR (842-918 nm)
- IEEE 802.3db VR (842-888 nm)
- IEEE 802.3db VR (842-868 nm)
- Fiber Channel PI - 7 Rev 0.13
- TDEC ITU 50G PON OLT
- TDEC ITU 50G PON ONU
Requires FlexDCA revision A.05.60 and above.