:MEASure:TDEQ:HWIDth
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEQ:HWIDth <unit_interval>
<unit_interval> is a double.
Query Syntax
:MEASure:TDEQ:HWIDth?
Description
Sets the width of the two histograms that are used to configure an Eye mode PAM4 TDECQ measurement (:MEASure:EYE:TDEQ command). Adjust this setting when FlexDCA is not in pattern lock. It adjusts the histogram window so that additional data can be acquired to decrease the measurement time.
| Setting | Range | Default Value |
|---|---|---|
| Histogram Width | 0.01 to 0.10 UI | 0.04 UI |
This command is equivalent to the Histogram Width setting which is located in the TDECQ Configuration tab of the PAM-N Analysis Setup dialog. To watch how the histograms change while you adjust this setting, display the histograms on the waveform.
The :MEASure:TDEQ:HWIDth command should always be followed with a *OPC? query for program timing.
Requires FlexDCA revision A.05.60 and above.