:MEASure:TDEQ:OHTHresholds
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEQ:OHTHresholds {ON | OFF | 1 | 0}
Query Syntax
:MEASure:TDEQ:OHTHresholds?
Description
Enables threshold optimization where you can move the thresholds of Eye mode's PAM4 TDECQ measurement (:MEASure:EYE:TDEQ command) from the standard definition. The thresholds can be moved by at most one percent of Outer OMA. To actually change the threshold value, use the :MEASure:TDEQ:TALimit command. By default, this setting is off.
This command is equivalent to the Threshold Optimization Enable setting which is located in the TDECQ Configuration tab of the PAM-N Analysis Setup dialog. The :MEASure:TDEQ:OHTHresholds command should always be followed with a *OPC? query for program timing.
Requires FlexDCA revision A.05.80 and above.