:MEASure:TDEQ:TALimit
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEQ:TALimit <percent>
Query Syntax
:MEASure:TDEQ:TALimit?
Description
Sets a limit to which thresholds can be moved from the standard definition.
The default value is 2 s. The minimum value is 1 s. The maximum value is 100 s.
Requires FlexDCA revision A.05.80 and above.