:MEASure:TDEQ:OHTLimit
Command Syntax
:MEASure:TDEQ:OHTLimit
Query Syntax
:MEASure:TDEQ:OHTLimit?
Description
Sets the histogram adjustment limit in UI for a :MEASure:EYE:TDECQ measurement. Before you can position the histograms, you must turn histogram time optimization on with the :MEASure:TDEQ:OHTime command. To adjust the time spacing in UI between the left and the right measurement histogram windows, use the :MEASure:TDEQ:OHSeparation command.
This command is equivalent to the Adjustment Limit setting which is located in the TDECQ Configuration tab of the PAM-N Analysis Setup dialog. To watch how the histogram changes while you adjust this setting, display the histograms on the waveform.
The :MEASure:TDEQ:OHTLimit command should always be followed with a *OPC? query for program timing.
| Setting | Range | Default Value |
|---|---|---|
| Histogram Adjustment Limit | 0.01 to 1 UI | 0.10 UI |
Requires FlexDCA revision A.06.60 and above.