:MEASure:TDEQ:PRESets
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TDEQ:PRESets <preset name>
<preset name> is a string.
Query Syntax
:MEASure:TDEQ:PRESets?
Description
Loads a preset for a TDECQ measurement (:MEASure:EYE:TDECQ). The preset configures the measurement to the proper settings. To query which presets are available for loading, use the MEASure:TDEQ:PRESets:SELections? query.
You can save your own presets from the measurements Setup dialog. There is no programming command for this task.
TDECQ Measurement Presets
- IEEE 802.3ds Draft 2.0
- IEEE 802.3dj Draft 3.3 DR (2km)
- IEEE 802.3dj Draft 3.3 DR (500m)
- IEEE 802.3dj Draft 3.3 FR4 (2km)
- IEEE 802.3dj Draft 3.3 FR4 (500m)
- IEEE 802.3dj Draft 3.3 LR4 (10km)
- CEI-112G-Linear
- IEEE 802.3dj Draft 2.3 DR (2km)
- IEEE 802.3dj Draft 2.3 DR (500m)
- IEEE 802.3dj Draft 2.3 FR4 (2km)
- IEEE 802.3dj Draft 2.3 FR4 (500m)
- IEEE 802.3dj Draft 2.3 LR4 (10km)
- IEEE 802.3bs Amended
- IEEE 802.3bs
- IEEE 802.3cd
- IEEE 802.3db
- Fiber Channel PI - 7 Rev 0.13
- Open Eye - VEC Statistical 2.0
- Open Eye - VEC Statistical 3.0
The preset includes the settings made with the following commands:
:MEASure:TDEQ:HWIDth(Histogram Width):MEASure:TDEQ:TSER(Target Symbol Error Rate)
Requires FlexDCA revision A.05.60 and above.
Example Commands
:MEASure:TDEQ:PRESet "CEI-112G-Linear" // Load a preset. :MEASure:TDEQ:PRESet:SELections? // Returns a list of presets.