:MEASure:TDEQ:OHSeparation
Command Syntax
:MEASure:TDEQ:OHSeparation <double>
Where <double> is the position in UI (unit interval).
Query Syntax
:MEASure:TDEQ:OHSeparation?
Description
Sets the time spacing in UI between the left and the right measurement histogram windows for a :MEASure:EYE:TDECQ measurement. Before you can position the histograms, you must turn histogram time optimization on with the :MEASure:TDEQ:OHTime command. To adjust the adjustment limit in UI between, use the :MEASure:TDEQ:OHTLimit command.
This command is equivalent to the Histogram Spacing setting which is located in the TDECQ Configuration tab of the PAM-N Analysis Setup dialog. To watch how the histogram changes while you adjust this setting, display the histograms on the waveform.
The :MEASure:TDEQ:OHSeparation command should always be followed with a *OPC? query for program timing.
| Setting | Range | Default Value |
|---|---|---|
| Histogram Spacing | 0 to 0.25 UI | 0.10 UI |
Requires FlexDCA revision A.05.80 and above.